Issue
Trying to access and display I/A Series R2 graphic pages from an Enterprise Server using my Blackberry that has Java ME installed on it but after logging in, nothing is displayed.
Environment
I/A Series R2 Enterprise Server or UNC graphics pages
Cause
The I/A Series R2 graphics are not compatible with the JavaME (Java Micro Edition or Java Mobile Edition) that comes pre-installed on the mobile device (smartphone).
Resolution
The full Java Runtime Environment (JRE) Version 6 is not available on any smartphones or tablet devices at this time. The I/A Series R2 graphics requires the use of the full JRE Version 6 and is not compatible with JavaME.