Repeating Index Entry

Issue

When scrolling down an Index, the same index entry repeats itself.

Product Line

Satchwell Sigma

Environment

Sigma

SigmaX

Cause

When scrolling down an Index, the same index entry repeats itself.

When creating software, the same index entry is constantly repeated.

Resolution

The index entry has been referenced to itself. This generally only happens during software creation and no pages are created at a lower level than the index entry in question.

1. In Sigmax goto Doctor Utility > Index Edit

2. Find the Index Entry in question

3. Either

Delete the page, only if there are no index entries after this.

or

determine where the page it is suppose to goto and change the page no. e.g.  BLD_HTP_        Heating Plant           0    0   22    0    0    0    0

The password to edit the index is ie