Where can I find help on TGML scripting and advanced features?

Issue

Where can I find help on TGML scripting and advanced features? Which javascript functions are supported and how do these impact performance.

Product Line

TAC Vista

Environment

TAC Vista TGML graphics editor 5.1.7

Cause

More advanced graphics often require scripting and the engineer needs to know which functions are supported.

Resolution

In the TGML editor under Help there is a section called TGML Format Specification. Details of scripting methods as well as examples can be found here.

 

Also check out the JavaScript Essentials - Episode 3 - Value Types Quick-Help video on the Exchange.