Can Satchsize the valve sizing software be used with Windows 7?

Issue

Can Satchsize the valve sizing software be used with Windows 7?

Product Line

Field Devices

Environment

Valve sizing

Satchsize

Cause

Customer wishes to use Satchsize on Windows 7.

Resolution

Satchsize is no longer available and is not supported with Windows 7, but a new program is available.

TAC Valve 1.8 UK can be downloaded from the Buildings Business Extranet. 

Once installed please use the help files installed with the program.