Issue
Is it possible to change the column size for the alarm window in Webstation? For some alarms it is not possible to see the whole alarm text for an alarm in the alarm window, he need to click on details to see the alarm text.
Environment
TAC Vista Webstation 5.1.x
Cause
The size of the columns is decided when the Webpage is built up and this is nothing that is possible to change in the Websettings.
Resolution
No this is not possible to change in the Websettings.