Issue
Override time remaining for Niagara Binary Override object
Environment
I/A Series R2 WorkPlace Pro
Cause
There is a need to know the override time remaining for an overridden Niagara R2 Binary Override object
Resolution
A RemainingOverrideTime object is available which can be connected to a Binary Override object to extract the override time remaining. The RemainingOverrideTime object can be found in 'tridiumx > lib > programObjects > hvac'.
- Binary Override object's overrideTime linked to the RemainingOverrideTime object's overrideTime input
- Binary Override object's statusInOverride linked to the RemainingOverrideTime object's statusInOverride input