What speed and duplex do the DMS and GCM Ethernet NIMs operate?

Issue

What speed and duplex do the DMS and GCM Ethernet NIMs operate?

Product Line

TAC I/A Series

Environment

DMS-ETH-001

GCM-ETH-001

Cause

Network troubleshooting

Resolution

Both NIMs (network interface modules) adhere to the IEEE 802.3 standard as written in the early 1990s.

The port speed is 10 Mbps at half-duplex.