Issue
Can a Netcontroller II be used to communicate directly to BACnet MS/TP devices?
Environment
BACnet MS/TP RS-485 XDriver
Netcontroller 2, NC2
bCX9640
Cause
No X Driver is listed for BACnet MS/TP.
Resolution
There is no X Driver available for the BACnet MS/TP protocol to allow a NC2 to communicate to 3rd party MS/TP devices.
However a bCX1 4040 can directly communicate to BACnet MS/TP on its Comm2 and is BTL listed to confirm compatibility.
Also a bCX1 9640 can be converted to a 4040 by flashing it with the 4040 flash file available on the Extranet.