SPP920 Datasheet, Technical Information and Installation Instructions

Issue

SPP920 Datasheet, Technical Information and Installation Instructions

Product Line

Field Devices

Environment

SPP920 Differential Pressure Switch

Cause

No information available for the SPP920. The Sensor catalogue says it is supported by Huba.

Resolution

Either click link www.hubacontrol.com and search for 630.

or the

Technical information can be downloaded here.

Installation Instructions can be downloaded here.

All of the various pressure range options come with the following options:

- EPDM diaphram material
- Brass Case
- Spec Cover PG9 - IP65 Rating
- Bracket Type A