Issue
Is it possible to change the colors for the alarm list in Webstation?
Environment
TAC Vista Webstation 5.1.x
Cause
The colors for the alarm list in Webstation are inherited from Vista Workstation.
Resolution
To change the colors for the alarm list in Webstation change the colors for the alarm list in Workstation and Webstation will inherit the colors.
Change the colors in workstation:
- Right click on a alarm in the alarm list and open the properties for it.
- Go to "Customize".
- Click on the "Text" tab.
- Change the color.
- Open the "File" menu and "Save My Program Settings"