Forta actuator only modulates 0-50% when given a 0-10V input signal

Issue

Forta actuator only modulates 0-50% when given a 0-10V input signal.  All DIP switches are OFF, so it should modulate 0-100% for 0-10V input.

Product Line

Field Devices

Environment

Forta

M800

Cause

If the X1 and MX control signal connections are reversed, the actuator will appear to modulate but the stroke will be limited to 0-50%

Resolution

Ensure that the actuator is correctly wired, according to the Forta datasheet.