Field Devices - What is the replacement actuator for the EM42?

Issue

What is the replacement actuator for the EM42?

Product Line

Field Devices

Environment

EM42

Actuator

Cause

The EM42 is obsolete.

Resolution

The EM42 actuator is generally associated with the V280/290, and the V380/390 series valves.

The replacement actuator for the EM42 is the Schneider Electric Forta M310 Actuator.

Please note that an adaptor kit (880-0252-000) is required for DN15 valves.

For a copy of the EM42 data sheet please click HERE.

For a copy of the M310 data sheet please click HERE.