Issue
Spare parts for V221
Environment
0804375005 Recond kit 221/223-65
0804376005 Recond kit 221/223-80
0804377005 Recond kit 221/223-100
0804538005 Recond Kit 221/223-125
0804627005 Recond kit 221/223-150
V221:
DN65 7212154000
DN80 7212158000
DN100 7212162000
DN125 7212166000
DN150 7212170000
Cause
Reconditioning kits for the V221 valves
Resolution
The following reconditioning kits are available until the end of 2012, after that they will be obsolete:
0804375005 Recond kit 221/223-65
0804376005 Recond kit 221/223-80
0804377005 Recond kit 221/223-100
0804538005 Recond Kit 221/223-125
0804627005 Recond kit 221/223-150