Issue
Want to create a listview that shows all expired personnel cards on or after today's date.
Environment
Cyberstation (all versions)
Cause
The built-in Personnel_Expired Cards listview does not have any date filters.
Resolution
Either edit the built-in Personnel_Expired Cards listview, or create a new on. Edit the listview, and click on the Qualifiers tab. Check the Advanced Database Qualifier box, and type the following expression in the Database field:
((ExpirationDate >=
where
When the listview is opened, cards expiring today and after will be displayed.