Issue
Do not know the card information such as card type, card number and site code.
Environment
CX99xx , CX 9680 , ACX57xx , ACX7xx.
Cause
Need to know the card information that is to be used and need to configure the door for the card to be used.
Resolution
- Set the door configuration to Site + Card mode.
- Open the Access EventView and swipe the card to the reader of the door.
- Verify the card information from Access EventView.