Issue
Some managed switches have settings that have to be configured to match the communications type and speed of the connected devices.
Environment
- Xenta 511, 527, 527-NPR, 555, 701, 711, 721, 731, 911, 913
Cause
Some managed switches have to be configured to match the communications type and speed of the connected devices.
Resolution
Most switches automatically detect the speed and configuration of the connected devices. However, for those site where these configurations must be manually configured, the specs below should be noted.
All Xenta Servers use a standard 10 Base T network port. These ports operate at 10 Mbits/sec. and are half duplex.