Issue
- Object type "Time Chart - Global" does not update local time schedule in a Xenta programmable controller.
Environment
- Vista 5.1.6 and below
- Xenta programmable controllers
- Xenta 281, 282, 301, 302, 401
Cause
After changing a "Time Chart - Global," changes are sent out to all time schedules located in the associated Xenta units. If the Xenta is busy when this update occurs, it can take too long for the update to arrive and a time-out happens. This causes the Xentas to not get updated.
Resolution
Various time chart/time schedule updates have been corrected in Vista 5.1.7 and more are to come in 5.1.8.
Please read the latest updates in the TPA