What are the valid Electrical Types for the smart input on a controller

Issue

What are the valid Electrical Types for the smart input on a controller

Product Line

Andover Continuum

Environment

b3, i2, smart

Cause

What are the valid Electrical Types for the smart input on a controller?

Resolution

Input X (SmartSensor) valid Electrical Types are:-
ACC_TEMP_DEGF
ACC_TEMP_DEGC
Digital

Note
If using a Smart sensor then ACC_TEMP_DEGF or ACC_TEMP_DEGC should be used
The temperature range is limited, so you can put a room temp sensor on OK, but not duct or pipe sensors as the temp range is 0-50DegC