Issue
The following error message is displayed in the UNC-s Standard Output Window when attempting to install a station:
FATAL: Cannot boot station from sns
java.lang.ClassNotFoundException: tridium.services.DatabaseService
Environment
Niagara R2, UNC-520, UNC-410
Cause
A UNC can not be licensed for DatabaseService.
Resolution
Open the station offline and remove the DatabaseService.