I/Net AMT error - Command Error

Issue

  • Command Error in AMT
  • MCU lost in AMT

Product Line

TAC I/NET

Environment

  • I/Net
  • AMT

Cause

If the I/Site loses contact with its SCU and there are a Global / Indirect point associated with this unit a Command error will appear in AMT.

Resolution

There can be various reasons for a SCU to go offline, it can be either power loss or grounding problem. Check the unit and the cables, it can also be that the unit is broken and needs to be changed.

Check TCON312 and TCON313 for installation help.