LonWorks Zone Controller SE7200F5545E

Issue

LonWorks Zone Controller SE7200F5545E

Product Line

TAC Vista, Field Devices, SmartStruxure Lite

Environment

Site requiring information or literature regarding this zone controller

Cause

Cannot find information on:
Part Number: SE7200F5545E
Part Name: ZNCTRL LONWORKS 2X0-10V PIR
Part Short Description: LonWorks Zone Controller :2 Analog 0-10V Outputs, PIR Cover Installed.
Part Long Description: LonWorks Zone Controller:2 Analog 0-10V Outputs with PIR Cover Installed

 

Resolution

Please find the following guides:

SE7000 Series Room Controller Brochure
SE7200 Series Room Controller Data Sheet
SE7200 Room Controller with Integrated PIR Motion Sensor Data Sheet
PIR Ready SE7200 Series Installation Guide
SE7200 and SE7300 Series LonWorks Integration Manual