Issue
Satchwell DuoFlow Information
Environment
DuoFlow
DM5601
SA2452
TLX2259
Cause
Drawing for a Satchwell DuoFlow System using a DM5601 valve and actuator.
Resolution
Download here drawing for a Satchwell DuoFlow system.
DuoFlow Valve/Actuator cable colours are as follows:
White = Central Heating
Orange = Hot water
Yellow = Mid Position (Central Heating and Hot Water)
Blue = Neutral
Note 1: The DuoFlow actuator wiring is different to a Mid-Position actuator, therefore conversion from a DuoFlow system is best done by replacing the wiring centre as well, The room and cylinder thermostat can be retained.
Note 2: The domestic valve and actuator part of the business is now part of SUNVIC.
Sunvic Controls Ltd.
General Enquiries :-
T: +44 (0) 1698 812 944
F: +44 (0) 1698 813 637
Email. enquiries@sunvic.co.uk
Technical Helpline :-
T: +44 (0) 1698 810 945
Email. technical@sunvic.co.uk