When were the different TAC Vista Server versions released?

Issue

  • When were the different TAC Vista Server versions released?
  • When was Vista Server version 4.X.X or 5.X.X released?
  • Need a list of release dates for TAC Vista Server
  • Need to know approximately how old a Vista site installation is

Product Line

TAC Vista

Environment

TAC Vista Server

Cause

It would be interesting to know the release date of the different Vista Server versions

Resolution

All the Vista release note documents are available on the The Exchange Download Center.

TAC Vista 3.11 - 1998-10-21
TAC Vista 3.21 Service Pack 1 - 2000-02-04
TAC Vista 2000 Server and Workstation 3.31 Service Pack 1 - 2001-07-04
TAC Vista 2000 Server and Workstation 3.32 - 2001-09-10
TAC Vista 2000 Server and Workstation 3.33 - 2001-12-20
TAC Vista 2000 Server and Workstation 3.33 SP2 - 2002-11-15
TAC Vista IV Server/Workstation/Menta 4.01 - 2003-02-21
TAC Vista IV Server/Workstation/Menta 4.10 - 2003-10-24
TAC Vista IV Server/Workstation/Menta 4.2 - 2004-03-10
TAC Vista IV Server/Workstation/Menta 4.2.1 - 2004-04-19
TAC Vista IV Server/Workstation/Menta 4.2.2 - 2004-06-24
TAC Vista IV Server/Workstation/Menta 4.2.3 - 2004-11-30
TAC Vista IV Server/Workstation/Menta 4.2.5 - 2005-03-21
TAC Vista Server and Workstation 4.3.0 - 2005-04-29
TAC Vista Server and Workstation 4.3.0 SP1 - 2005-05-25
TAC Vista Server and Workstation 4.3.1 - 2005-07-15
TAC Vista Server and Workstation 4.3.1 SP1 - 2005-10-31
TAC Vista Server and Workstation 4.4.0 - 2005-12-16
TAC Vista Server and Workstation 4.4.1 - 2006-03-13
TAC Vista Server and Workstation 4.4.2 - 2006-05-29
TAC Vista 4.5.0 - 2006-07-05
TAC Vista 5.0.0 - 2006-11-15
TAC Vista 5.0.1 - 2007-04-26
TAC Vista 5.0.2 - 2007-09-28 (first version to support Xenta 700)
TAC Vista 5.0.3 - 2008-01-21
TAC Vista 5.1.0 - 2008-06-03
TAC Vista 5.1.1 - 2008-10-27
TAC Vista 5.1.2 - 2009-04-15
TAC Vista 5.1.3 - 2009-09-24
TAC Vista 5.1.4 - 2010-03-31
TAC Vista 5.1.5 - 2011-01-25
TAC Vista 5.1.6 - 2011-07-04
TAC Vista 5.1.7 - 2012-01-03

Note: All dates are in the form [year]-[month]-[date]