Sigma Integration to Simplex Fire Alarm Panel

Issue

Sigma Integration to Simplex Fire Alarm Panel

Product Line

Satchwell Sigma

Environment

Satchwell Sigma Integration

Cause

A Simplex PIU was available in Satchwell BAS system but there is no Simplex Integration Controller in Sigma

Resolution

Simplex has a BACnet Ethernet module supplementary communications interface that converts data from a compatible Simplex fire alarm control panel into the BACnet protocol.
Refer to Lessons Learned Article #6767 for details on Sigma integration to BACnet.

Alternatively, a 3rd party gateway / interface can be used. Field Server Technologies has gateways (LonWorks, BACnet, Modbus etc.) for SimplexGrinnell 4020 Fire Alarm Panel and SimplexGrinnell TFX 500/800 Fire Alarm Panel. Contact Field Server Technologies directly for sales and technical enquiries.