Issue
Operation of the "Speed Clock" facility.
Environment
Drayton
DC1100
DC1400
DC1100/1400
Speed Clock
Cause
Information on the enabling/disabling of the "Speed Clock" function.
Resolution
The "Speed Clock" function on the DC1100/1400 controller allows the user to test the controllers timed functions in a short period of time. It is enabled / disabled as follows;
Rotate the controller rotary switch to "SET".
Navigate through the menu structure to "System Menus / Alter Settings / Enter Password, and enter a password of 0402.
Choose either to "Enable" or "Disable".
Return the rotary switch to "Auto" to run the test.