Why is there a bluish tint to the IS90 Camclosure?

Issue

Why is there a bluish tint to the IS90 Camclosure?

Product Line

Pelco Cameras

Environment

IS90 Series Camclosure

Cause

Cameras positioned in direct lighting conditions, such as sunrise and sunset, may exhibit a bluish tint to the video.

Resolution

 Take the following steps to correct the issue:

  1. Place the camera at a different location or angle so that it is not directly in view of the light source.
  2. Replace with a new CH or DN model IS series camera - the bluish tint condition occurs in a low percentage of the cameras that are produced.
  3. Replace the camera with an IS series wide dynamic range camera. The wide dynamic color (CW) and day/night (DW) models are optimized for extreme lighting conditions.
  4. Use the DN and CH series camera indoors only.