How do I change the boot sequence or boot priority in the DVR5100 series BIOS?

Issue

How do I change the boot sequence or boot priority in the DVR5100 series BIOS?

Product Line

Pelco Video Management

Environment

DVR5100 series recorder

Cause

Change the order devices are boot.

Resolution

To change the boot sequence in the DVR5100 the following steps can be followed.
 
  1. Connect a USB keyboard to the DVR5100.
  2. Power on the DVR5100.
  3. During the boot process tap the DEL key once a second until the BIOS menu appears.
  4. Select Advanced BIOS Features.
  5. Select Hard Disk Boot Priority.
  6. Use the +/- keys on the keyboard ten-key pad to reorder the devices.
  7. Press F10 to save and exit the BIOS.