Can multiple EE500 EnduraXpress series network video recorder reside on the same network or VLAN?

Issue

Can multiple EE500 EnduraXpress series network video recorder reside on the same network or VLAN?

Product Line

Pelco Video Management

Environment

Endura EE500- All versions

Cause

Information regarding the functionality of having two EE500s on the same network is needed.

Resolution

No. The EE500 was designed to be a stand-alone system. Multiple EE500 should not be in the same network as they will conflict due to similar services running on the EE500.