What is the maximum USB cable length that can be used to connect the KBD5000 keyboard to the DVR5100 series or Endura VCD5202?

Issue

What is the maximum USB cable length that can be used to connect the KBD5000 keyboard to the DVR5100 series?

Product Line

Pelco Video Management

Environment

  • DVR5100 Series HVR
  • Endura VCD5202
  • KBD5000 keyboard

Cause

Extend the length between the DVR5100 recorder and KBD5000 keyboard.

Resolution

The maximum USB cable length for the DVR5100 utilizes the USB full speed specification of 5 meters (16.4 feet).