How do I subscribe/unsubscribe from alarm event notifications using Endura WorkStation?

Issue

How do I subscribe/unsubscribe from alarm event notifications using Endura WorkStation?

Product Line

Pelco Video Management

Environment

Endura WS5000- All versions

Cause

Procedure on how to unsubscribe from alarm notifications is needed.

Resolution


To subscribe/unsubscribe to alarm event notifications you must first be logged in as administrator then do the following:

  1. Enter the Setup menu
  2. Click on the Users tab and select the user you wish to subscribe/unsubscribe alarms for.
  3. Check the appropriate severity Display warning for alarms with severity dialog box.
  4. Click Apply.
  5. Changes will take affect the next time that user logs in.

Note: If the same user is logged into the VCD5000 video console display, the user must logout and login to subscribe/unsubscribe from event notifications.