Is Endura Mapping version 1.0 or 2.0 compatible with DVR5100 series?

Issue

Is Endura Mapping version 1.0 or 2.0 compatible with DVR5100 series?

Product Line

Pelco Video Management

Environment

  • Endura Mapping- All versions
  • Endura DVR5100- All versions

Cause

Information on the compatibility of Endura Mapping with the DVR5100 series is needed.

Resolution

No. Endura Mapping is not compatible with DVR5100 series. It is only compatible when the DVR5100 series is in the Endura Enabled state and integrated into an Endura System.