How do I program camera configuration settings in the DVR5100 series?

Issue

How do I program camera configuration settings in the DVR5100 series?

Product Line

Pelco Video Management

Environment

DVR5100 series hybrid video recorder (HVR)

Cause

Navigate to cameras tab to configure camera settings.

Resolution

To access cameras settings directly from the DVR5100:
  1. Log on using an administrator account.
  2. To access the System setup screen, press the “M” key [or Menu button] to display the Main menu
  3. Click Setup [or press the red function button ]. The System setup screen appears.
  4. Select the Cameras tab. The Cameras screen appears.
  5. Click desired camera. The current settings for that camera is displayed and can be changed.