Issue
Can I swap varifocal lenses on the IS151-CHV9 camera?
Product Line
Pelco Cameras
Environment
IS151-CHV9
Cause
The IS series lenses are designed for there specific model assembly.
Resolution
Lenses are not interchangeable. If the lenses require to be changed to support the view of interest, it requires the purchase of a new camera model.