What are Minimum System Requirements to control Spectra IV IP?

Issue

What are Minimum System Requirements to control Spectra IV IP?

Product Line

Pelco Cameras

Environment

  • Spectra IV IP

Cause

Perform PTZ (Pan, Tilt, Zoom) functions from a PC computer.

Resolution

Minimum System Requirements:

Processor Intel® Pentium®  4 microprocessor, 1.6 GHz
Operating System Windows® 98, Windows 2000, Windows XP (or later), or Mac® OS X 10.3.9 (or later)
Memory 512 MB RAM
Network Interface Card 100 megabits
Web Browser Internet Explorer 5.5 (or later); Mozilla® Firefox® 1.5 (or later)
Monitor Minimum of 1024 x 768 resolution, 16- or 32-bit pixel color resolution