Programming procedure to alternate between NTSC/PAL composite, NTSC/PAL S-Video, or VGA monitors on the DVR5100 series recorder.

Issue

What is the programming procedure to alternate between NTSC/PAL composite, NTSC/PAL S-Video, or VGA monitors?

Product Line

Pelco Video Management

Environment

DVR5100 series hybrid video recorder (HVR)

Cause

Change video output on the DVR5100 recorder from VGA to composite or S-Video monitor.

Resolution

The default DVR5100 monitor configuration is VGA. If you are using a composite or S-Video monitor, change the output mode as follows:
• At startup, press the yellow function button for NTSC or the green function button for PAL. The unit will restart in a composite monitor output mode.