Reset the Endura NET5301T encoder to factory default

Issue

How do I reset the Endura NET5301T encoder to factory default?

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

  • Endura NET5301T- All versions
  • Endura WS5000- All versions

Cause

A reset to factory defaults is needed.

Resolution

  1. Enter the Setup menu in the WS5000 software.
  2. Click on the Devices tab.
  3. Filter 'Device Type'  to Encoder
  4. Highlight the Encoder in the 'Device' column that will undergo a factory reset
  5. Using the mouse, right-click and choose the 'Restore Factory Defaults' option