Cameras attached to NET5300T series encoders show one hour off after DST Change.

Issue

Cameras attached to NET5300T series encoders show one hour off after DST Change.

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

Endura NET5301T- Versions below 1.3.1059

Cause

Lower versions of software are unable to keep the time in sync after DST.

Resolution

Prior to Day Light Savings (DST) the NET5301T encoders should be updated to version 01.03.1059 or higher to keep time in sync after DST.  If DST however did occur and the NET5301T encoders are at a previous version, the NET5301T encoders should under go a reboot to resync time.  Thereafter, update the NET5301T encoders to version 01.03.1059 or higher to prevent future occurrences.