What are the minimum system requirements for the Sarix IE Series?

Issue

What are the minimum system requirements for the Sarix IE Series?

Product Line

Pelco Cameras

Environment

  • Sarix IP Cameras

Cause

Minimum requirements to view Sarix IP cameras

Resolution

Minimum System Requirements:
 

Processor

Intel®, Pentium® 4 microprocessor, 1.6 GHz

Operating System

Microsoft® Windows® XP, Windows Vista®, or Mac® OS X 10.4 (or later)

Memory

512 MB

Network Interface Card

100 megabits (or greater)

Monitor

Minimum of 1024 x 768 resolution, 16- or 32-bit pixel color resolution

Web Browser

Internet Explorer® 7.0 (or later) or Mozilla® Firefox® 3.5 (or later);
Internet Explorer® 8.0 (or later) is recommended for configuring analytics.

Media Player(*)

QuickTime® 7.6.5 for Windows XP, Windows Vista, or QuickTime 7.6.4 for Mac OS x 10.4
(Internet Explorer is not supported by Mac OS x 10.4)

(*) This product is not compatible with QuickTime version 7.6.4 for Windows XP or Windows Vista. If you have this version installed on your PC, you will need to upgrade to QuickTime version 7.6.5