What are the PTZ protocols options for Endura NET5301T, NET5301T-I, or SP040-140 video encoders?

Issue

What are the PTZ protocols options for Endura NET5301T, NET5301T-I, or SP040-140 video encoders?

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

Endura NET5301T/NET5301T-I/SP04-140- All versions

Cause

Need to know which PTZ protocols are supported.

Resolution

By default the PTZ control mode is set to Disabled. Some PTZ protocols options in which the encoder support are Coaxitron, Extended Coaxitron, Pelco P, or Pelco D (RS-422) for a PTZ device.