Is the KBD5000 keyboard compatible with the Endura WS5050, WS5060, and WS5070 workstations?

Issue

Is the KBD5000 keyboard compatible with the Endura WS5050, WS5060, and WS5070 workstations?

Product Line

Pelco Video Management

Environment

  • Endura KBD5000- All versions
  • Endura WS5000- All versions

Cause

Information regarding the compatibility of the KBD5000 with the WS5000 is needed.

Resolution

Yes, however it is limited in functionality.

Supported Functions

  • PTZ control
  • Activating presets
  • Calling up cameras by number
  • Rewinding from live.
  • Switching workspaces
  • Activating auto-scan

Functions not supported

  • No monitor wall control
  • The red button has no functionality