What are the hard drive replacement part numbers for the DX8100 Series Hybrid Video Recorder?

Issue

What are the hard drive replacement part numbers for the DX8100 Series Hybrid Video Recorder?

Product Line

Pelco Video Management

Environment

DX8100 Series HVR

Cause

Replace failed hard drive.

Resolution

As of December 2010, the Hard Disk Drive upgrade part numbers for the DX8100 Series HVR are -

DX81HDD250KIT DX8100 SATA 250 GB upgrade
DX81HDD500KIT DX8100 SATA 500 GB upgrade
DX81HDD750KIT DX8100 SATA 750 GB upgrade
DX81HD1000KIT DX8100 SATA 1000 GB upgrade
DX81HD1500KIT DX8100 SATA 1500 GB upgrade
DX81HD2000KIT DX8100 SATA 2000 GB upgrade is no longer available, you can use part number EE11-0002-2011.


The latest hard disk drive upgrade part numbers can be found on the DX8100 Specification Sheet .

A total of four hard drives can be install in a DX8100 Series.

For more information on replacing failed hard disk drives, contact Pelco Product Support at 1-800-289-9100 or via email at techsupport.pelco.com.

*Hard drives must be ordered from Pelco. 3rd party drives are not supported.