What is a pattern?

Issue

Pattern

Product Line

Pelco Cameras

Environment

PTZ (Pan Tilt Zoom) cameras

Cause

Information about the pattern feature in Pelco PTZ cameras.

Resolution

A pattern is a set of memorized, repeating series of pan, tilt, and zoom movements that can be recalled by the device. The number of patterns that can be recorded and activated is dependent on the device. For example, the 16X and 18X models of the Spectra IV can store only a single pattern, while the 22X, 23X and 35X Spectra IV models can store up to eight patterns.