What are the viewing display options for the Esprit with Thermal Imager?

Issue

Viewing display options for the Esprit with Thermal Imager

Product Line

Pelco Cameras

Environment

Esprit with Thermal Imager

Cause

Views on Esprit with Thermal Imager

Resolution

There are 12 display type programs. The specific palette of colors to represent the temperature in the thermal image. These colors are not calibrated to a specific temperature. Rather, they represent the temperature variations within the thermal image.