Is a KBD300A required to select programming on the Esprit w/Thermal Imager?

Issue

To select programming on the Esprit w/Thermal Imager Is a KBD300A required?

Product Line

Pelco Cameras

Environment

KBD300A

Cause

Programming Esprit

Resolution

If the KBD300A is going to be the device to control the unit directly, then yes. It has the capability to communicate in either D or P protocol over twisted pair to unit and will be able to access the menus to do any programming.