What is the thread size used for the ID-P?

Issue

What is the thread size used for the ID-P?

Product Line

Pelco Cameras

Environment

ID-P (Pendant mount adapter)

Cause

Mating parts with the ID-P

Resolution

The ID-P is a pendant mount adapter specifically designed for ID and IDE Series network dome cameras. The pendant adapter modifies the network camera for pendant installations using a 1.5-inch (3.81 cm) NPT mount, such as the SWM-WT mount. The 1.5-inch (3.81 cm) NPT pipe is compatible with most mounting options that meet the NPT mounting specification.