Mount the Sarix ID series indoor dome inside a DF5 series in ceiling back box.

Issue

How can I mount the Sarix ID series indoor dome inside a DF5 series in ceiling back box?

Product Line

Pelco Cameras

Environment

  • Sarix ID indoor dome
  • DF5 Series Back Box

Cause

Add IP cameras to current installed DF5 housings.

Resolution

The ID-DF5 adapter kit is required to insert the Sarix ID series indoor dome inside a DF5 Series back box.
Note: The adapter kit is used for the ceiling model only.

Click Here to view ID-DF5 Installation Manual