Is it possible to discover all the cameras attached to an Endura system, and their associated camera number?

Issue

Is it possible to discover all the cameras attached to an Endura system, and their associated camera number?

Product Line

Pelco Video Management

Environment

Endura system- All versions

Cause

Information on how to discover all Endura cameras and numbers is needed.

Resolution

The System Manger Wrapper allows users to more easily utilize System Manager related functionality. It allows the retrieval of attribute information for all devices such as model number, available services, friendly name, device type, and so on. The clients will be able to integrate this wrapper to get device information which could then be used for doing playback, live streams, and so on.

Please refer to Lessons Learned Article #8888, Pelco API SDK's System Manager Wrapper, for more details.