What is the maximum number of simultaneous connections or users supported on the DX4100 series?

Issue

What is the maximum number of simultaneous connections or users supported on the DX4100 series?

Product Line

Pelco Video Management

Environment

DX4100
DX4100 Series Client
DX Series Client
DS Control Point

Cause

DX4100 is built to only support 5 concurrent users.

Resolution

The maximum number of simultaneous connections or users supported on the DX4100 Series DVR is 5.