Will the Spectra IV IP work on DC or AC voltage?

Issue

Will the Spectra IV IP work on DC or AC voltage?

Product Line

Pelco Cameras

Environment

  • Spectra IV IP series

Cause

Information on the supported current (direct current, alternating current) on the Spectra IV IP series.

Resolution

The Spectra IV IP can be connected to either 24VAC or 24VDC.