How to determine a Sarix camera's firmware version

Issue

How do users determine a Sarix camera's firmware version?

Product Line

Pelco Cameras

Environment

  • Sarix
  • IP Cameras

Cause

Firmware version currently running to determine if an upgrade is required.

Resolution

  1. Login to the Sarix camera's web application.
  2. Next, click on the Settings link on the top left.
  3. Now the System tab's contents should be viewable. If not click on the System tab. The firmware version number should be on the bottom left of the screen.